cancel
Showing results for 
Search instead for 
Did you mean: 

Got the following error when I tried to click on the .bat file generated by eDesignSuite. No value found for registry key: "HKEY_CLASSES_ROOT\SIMetrixSchematic\shell\open with STMicroelectronics eDSim Electrical simulator\command"

EHD
Associate II
 
7 REPLIES 7
Patrizia BELLITTO
ST Employee

Hello!

Could you give more details? Which design are you using? Can you share here the zip file you are downloading from eDesignSuite?

Thanks

Patrizia

EHD
Associate II

Hi Patrizia,

Attached is the zip file, all I did was click on the eDSim bat file, and the cmd window popped up with that error message. Thanks.

Patrizia BELLITTO
ST Employee

We were able to start the simulation without problems. Which eDSim version do you have? Does it happen only for this bat file or even with other export?

It is the newest. I do have issues with python installation (wait for IT to approve), will that cause the issue?
Ellen Ding
Expert Field Applications Engineer
T: +1 617-992-0568
E: ellen.ding@arrow.com
Arrow Electronics | arrow.com
Patrizia BELLITTO
ST Employee

If that value in the registry is empty, maybe the eDSim installation has been done and completed with a different user respect to that one you are using now to lauch the .bat file. Could you verify?

Thank you, it is all good now.

Ellen Ding
Expert Field Applications Engineer
T: +1 617-992-0568
E: ellen.ding@arrow.com
Arrow Electronics | arrow.com
Marco FICHERA
ST Employee

Hi @EHD​ ,

you should see something like this in your registry:

0693W00000Y9ciAQAR.png 

With the reg key reporting something like this:

"C:\Program Files\eDSim-850\bin64\SIMetrix.exe" "%1"

Regards

Marco