Hi,I have STM32WB55RG and GNSS1A1 boards. I am trying to run SimOSGetPos example however my GNSS1A1 module returns only empty messages. As far as I was able to troubleshoot, I found function GNSS_PARSER_ParseMsg which enters infinite loop that is loo...
Could you tell me MTBF and FIT of PARTS1.STB120NF10T42.SMLVT3V3
Dear Sir/Madam,Using ST490ABDR IC as RS485in the Weather Monitoring project. The device is not working with multiple MODBUS slave. I observed signal level on the Oscilloscope, it is dropped at the time of query. Please find attached Schematic and wav...
Hi,I have two X-NUCLEO-GNSS1A1 expansion boards.I powered on the first board, and connected to UART port. I can read GPS messages from the board. GPS location is good. (I got GPRMC and GPGGA, GPGLL, etc.) I don't know what I did. Somehow NMEA messag...