cancel
Showing results for 
Search instead for 
Did you mean: 

Write FLASH from RAM

smartpocket
Associate II
Posted on January 01, 2008 at 16:58

Write FLASH from RAM

12 REPLIES 12
smartpocket
Associate II
Posted on December 06, 2004 at 10:41

Hi,

this is the orinigal project of Bouha, whit some modification.

If executed step by step it work, but in normal run mode the micro stop at undefined opcode.

regards

smart

________________

Attachments :

WriteFlashTest.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtTO&d=%2Fa%2F0X0000000aQS%2FQuiJJLtEga24HlEpQzopWNHN34DWEPyKH1ltPOBzKnE&asPdf=false
jkwon
Associate II
Posted on June 25, 2005 at 01:01

I have one more question regarding your question.

The mechanism is on Realview. I wonder the same mechanism can be applied on Keil. If yes, can I have the library based on Keil?

If you have any libray, please provide me even if it is simple.

I ask you to check IAP program based on KEIL. If yes, I'd like to get the library also.

I'm looking forward your kind reply.

charhenmal
Associate
Posted on January 01, 2008 at 16:58

Is there already an flash library or example

available for STR731 with RIDE.

Regards,