cancel
Showing results for 
Search instead for 
Did you mean: 

wiring diagram and other info

kalpaknirale
Associate II

i need help with a project, mainly wiring diagram and other information. I have sent components images 
i need to wire up two stm32f103c8t6 to 
1. 5 4-pin tact switch 

2. 3 5-way tactile switch 

3. 5 3-way toggle switch (6-pin)

4. 2 wh148 10k potentiometer with knob 

5. 1 ps2 joystick module breakout sensors (5v, push button when pressed down, Rx-Ry)

6. 4 ss49e analog hall effect sensor 

7.10pF 50v ceramic capacitors dip  ( please tell me how many to use )

8. 1N4148 1W zener diode 

I will need to make all this wired up on first stm32f103c8t6 

 

and on the second stm32f103c8t6  i need to wire these components 

1. 4 4-pin kd4-22n push button switch dpst with lamp

2. 4 4-pin rocker switch with lamp 

3. 8 3-pin 2 way toggle switch 

4. 2 a10k potentiometer 3-pin

5. 1 100k potentiometer 3-pin 

 

this is my first stm32 project soo any additional information will be very useful 

Thanks You 

 

2 REPLIES 2
kalpaknirale
Associate II

also can the tactile switch be used as button matrix 

 

Andrew Neil
Evangelist III

@kalpaknirale wrote:

i need help with a project, mainly wiring diagram and other information.


Are these not part of your project - ie things that you need to do?

Are you designing your own boards, or using ready-made?

Even if you will eventually be designing boards, you should start on development boards to prove your design.

NUCLEO-F103RB should be suitable:

https://www.st.com/en/evaluation-tools/nucleo-f103rb.html 

Schematics are available on the 'CAD Resources' tab:

https://www.st.com/en/evaluation-tools/nucleo-f103rb.html#cad-resources

You can see examples of using switches there...

 

If designing boards, study AN2586Getting started with STM32F10xxx hardware development:

https://www.st.com/resource/en/application_note/an2586-getting-started-with-stm32f10xxx-hardware-development-stmicroelectronics.pdf

Also take a look at the other Application Notes available on the Product Page:

https://www.st.com/en/microcontrollers-microprocessors/stm32f103rb.html#documentation