cancel
Showing results for 
Search instead for 
Did you mean: 

Which board has....

zhenhua0197
Associate
Posted on November 28, 2008 at 10:42

Which board has....

3 REPLIES 3
zhenhua0197
Associate
Posted on May 17, 2011 at 09:56

Hi all, as a student getting started to learn embedded (Linux) system, I'm looking for a nice development board, which embodies a 32bit ARM9 processor and some useful connection (USB, 2 or 3 serial, ethernet, camera...). For me as a beginner, I need it to be ready to run and inexpensive (<=$300), pre-configured tool chain and necessary binaries, example projects included.

better would it be if it has been attached with a LCD

Thanks in advance for any information that would be helpful.

jon2399
Associate
Posted on May 17, 2011 at 09:56

You may would like to check the

http://www.developmentboard.net/index.php/productdetail/Development+boards/ARM9/SAMSUNG/S3C2440/MINI2440+with+LCD

from

http://www.developmentboard.net

ARM920T CPU

64M SDRAM+64M NAND FLASH+2M Nor Flash

USB HOST and device

3 serial ports

SD card slot

3.5'' TFT LCD

...

Price=€200= about $251

seems a great board, I have bought it 2 days ago and will get it soon :) :-D

dhoyen
Associate II
Posted on May 17, 2011 at 09:56

hi,

I m not an expert about embedded linux, but seems need a external memory controler, with ''huge'' quantity (in comparaison to the STR9 embedded 96K of RAM). Same idea with flash.

Take a look with Atmel, they make some ARM9 at 180-200 Mhz (i forget the name of these device), really well supported by linux and the community and with plenty of documentation as / how tu use GCC, linux...

Good luck.