cancel
Showing results for 
Search instead for 
Did you mean: 

What kind of diode I am seeing here

K76
Associate

Good morning to everyone!!

I own a Hps 125A single phase welding machine and the diode has blown and I can't read the part number.The input voltage in my country is 240v  and 50hz.

I am attaching a photo of the component maybe can help

Thank you

IMG_20231221_104850.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
2 REPLIES 2
xisco
Associate III

Unfortunately, the BYV52 dual rectifier and the package have long since been discontinued without replacement. However, you could try the STTH6002CPI as a replacement, although it has a slightly lower surge non repetitive forward current.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.