2007-03-15 08:53 PM
what is the function of the Clock Configuration Register (ENET_CCR)
2011-05-17 12:39 AM
Hello!what is the function of the Clock Configuration Register (ENET_CCR),I can not find the code refer to the register in the ENET library.who can help me ?Thank you!
2011-05-17 12:39 AM
Hi sunshan,
It's not important to configure ENET_CCR register because the DMA units are located only on the AHB bus and not on the APB.In fact, this register have its reset value (HCLK=PCLK). With best regards, mirou2011-05-17 12:39 AM
Thank you!can you look at the message which title is ''the perplexity about the MAC/DMA Controller with DMA''.