2009-12-16 11:51 PM
Using IAR / J-Link to Write bank1
2011-05-17 12:45 AM
Hi,
I have used CAPS tool and R-Link to change the Boot order from bank0 to Bank1 I am using IAR IDE + J-Link, By default the IAR download the application to Bank0, How can I download the application to bank1 using IAR ? Thanks2011-05-17 12:45 AM
Usatyj,
Could you POST your modified files that load both Banks. Thanks, Rhys2011-05-17 12:45 AM
I downloaded yesterday the IAR 5.0
In this release there are some samples related with this kind of problems I hope to tell you something more in the next days.2011-05-17 12:45 AM
I use IAR 4.30. There is source code of flashloader, which load Bank 0.
I add piece of code, which load Bank 1 (like Bank 0 but another addresses and sectors size), and now use this loader for all projects.2011-05-17 12:45 AM
Hi.
I want to find Boot Loader (Simmilar IAP) in IAR + J-Link. But, I don't know how i write to bank1 of flash. So, I want to need your code. Please, let me send your source code(Usatyj)! Please... Help me!2011-05-17 12:45 AM
The STR91x Flash loader included in the latest version of IAR(EWARM5.11) supports the 2 bank 0 & 1 and it detects automatically which bank is @ 0x0.
So remap the bank 1 to address 0x0, and link you code to 0x0 then the loaded code will be put in bank 1. Rgds2011-05-17 12:45 AM
Hi all,
to set the bank 1 as the boot bank on the st9 using jlink, you can use the Segger j-link tools. you can find them here: open the folder with command line and call jlinkstr91x.exe. it should connect through jlink. you then have to type 'setb 1' and you're done. the boot bank will be the bank 1. hope it helps! cheers, Bib'