2008-11-02 04:52 PM
2011-05-17 02:52 AM
Hello,
I am develop an application on uPSD3454EV for In-Application Programming (IAP) using USB. i use our own USB drivers developed on WinDDK and well tested on ARM system, firmware for uPSD3454EV for both boot loader and application is written in the C language and complied using keil uVision3 compiler and PC side software is developed in Visual C. I am face problem regarding its reliability means if we download firmware in the uPSD3454EV controller 50 times using my USB IAP it is ok ( means full downloading is complete ok and device work functionally ok ) nearly 25 times only and other times it is failed. i test this on 4 to 5 different PC but i get same result. And when downloading is not ok it stop download at somewhere and pc side software give me error. Error: A device attached to the system is not functioning. please give me documents if anyone find such problems and solution on it, or some extra care which i want to take which is not given in datasheet of uPSD34xx, or give some probable reason because of it may happen. Waiting for your replay. Thank You. Somnath H. Jagtap