cancel
Showing results for 
Search instead for 
Did you mean: 

USB Bulk transfer.

paulbrown9
Associate II
Posted on January 17, 2006 at 04:00

USB Bulk transfer.

17 REPLIES 17
fa
Associate II
Posted on December 19, 2005 at 10:10

Hi Iamanil

Sorry but I have not got any further with this problem, and I have also posted another request in this forum, but I get no answers.

It is still a problem for me to get read bulk to work correctly.

Best regards,

Frank Andersen

reg007
Associate II
Posted on January 03, 2006 at 09:19

hmmm.

I think this is my Problem too.

Has anyone a solution?

regards

anil23
Associate II
Posted on January 03, 2006 at 11:46

Nops...not moved any further...

reg007
Associate II
Posted on January 11, 2006 at 06:23

damn..... :-Y

I solved my Problem.

There was a bug in the Windows XP (SP1) USB Module.

I patched it, an everything works fine. :o

Be sure to have

http://www.microsoft.com/downloads/details.aspx?FamilyID=733dd867-56a0-4956-b7fe-e85b688b7f86&displaylang=de

installed if your working on WinXp with SP1.

regards

gajeronline
Associate II
Posted on January 11, 2006 at 11:16

Hi Guys.

I downloaded bulkusb-ddk.zip, and I have a question, where I can find SDK for this source.

I try compile this source in borland c++, but compilation faild, becouse t i don't have devioctl.h setupapi.h usbdi.h.

anil23
Associate II
Posted on January 11, 2006 at 11:22

Hey re-G,

Thanks for the update. I'm on a Win XP SP2 machine. I believe that this update wouldn’t work for me. Can you please forward me the example source code of the bulk transfer.

Regards,

mohamed23
Associate II
Posted on January 16, 2006 at 15:00

Hi All,

Jungo has a solution named WinDriver that allows one to access a USB device and so send or receive data on pipes directly from User mode.

So you can develop your STR71x USB firmware ( Control/Interrupt/ Bulk/ isochronous) and test it with this Software PC solution in all Windows platforms.

have a look to www.jungo.com

Rgds

:o :o :o

reg007
Associate II
Posted on January 17, 2006 at 04:00

Thx Rave.

I'm working with the USB Dev Driver, developed by

http://www.thesycon.com

.

It seems like beeing the same as jungo provides.

But thx for the link.

@ianmali

This is only a bug of SP1. I don't think this patch will work on SP2, sry.

regards