2006-01-16 07:00 PM
2004-11-29 05:51 AM
I have managed to get bulk transfer from host to STR711, but cannot get the other way working. I have set up EP2 as a bulk out in the usb_desc.c file and created a callback Callback_ep2. But the callback does not seem to get called. In fact I can't seem to get any USB interrupt that use EP2.
Do I need to set something else up first. For instance I have initialised a buffer for receiving the data with the following SetEPRxAddr(ENDP2, ENDP2_RXADDR); SetEPRxCount(ENDP2, 32); SetEPRxValid(ENDP2); but don't know if this is the correct thing to do. Please help P.2005-08-30 12:28 AM
Could you also give us a version for IAR 4.30? There seems to be quite a lot of code to change and it would be easyer for you to do it... I'll try to do it myself, hope to make it work.
2005-10-12 01:14 AM
Hi.
Just one question, Risc. Did you develop the ''RwBulk.exe''? And if so, may i get the source code, or better might you give me the programing interface for the Driver? I am not able not find the documentation fo the driver on www.intel.com. Thanks for your help. Regards re-G [ This message was edited by: re-G on 12-10-2005 13:45 ]2005-10-12 05:07 AM
it all all taken from the windows ddk samples - attached
Regards sjo ________________ Attachments : bulkusb-ddk.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtJz&d=%2Fa%2F0X0000000aLa%2FWB9WRyaNySq1H5n3RTZCtioAQA8u4w6SsF4XSd6j5mM&asPdf=false2005-10-13 07:58 PM
Quote:
On 30-08-2005 at 13:36, Anonymous wrote: Hi, I have attached a version of the USB bulk for EWARM 4.30A regards, zouhair has anybody keil arm version of the USB bulk ?2005-10-13 08:06 PM
@ RISC: nevermind :-D
@ sjo: thanks for the example. regards2005-11-08 10:34 PM
[EDIT]
Sry. Question answered. Finaly i've found it. :-] [/EDIT] [ This message was edited by: re-G on 09-11-2005 15:26 ]2005-12-01 01:12 AM
Hi,
I am trying to get the Bulk example to work, I am able to get the readbulk working once, then no interrupts occurs. The write functions seems to work, but I havn't been able to verify that the write actually takes place on the MCU. Best regards, Frank Andersen [ This message was edited by: frankandersen on 01-12-2005 15:42 ]2005-12-16 09:57 AM
Hi Frank,
I'm stuck at the same problem as you are...Could you get usb work any further...If so...please advise me.... Thanks.....