2003-11-19 04:26 PM
2011-05-17 02:56 AM
I'm using two uPSD. One of them is master and the other is slave .
I use Keil C. There are no problem to work except one. That is to declare a data type in slave . If I declare a variables for using S2DAT in idata, It is no problem. But I do in xdata, it does'n work. for example unsigned char xdata buff[10]; does'n work; unsigned char idata buff[10] ; OK There is no problem like that in master just slave . How can I fix it.mailto:null