cancel
Showing results for 
Search instead for 
Did you mean: 

Systemclock programming (PRCCU-Block) problems

jhaug9
Associate II
Posted on December 17, 2004 at 10:22

Systemclock programming (PRCCU-Block) problems

1 REPLY 1
jhaug9
Associate II
Posted on December 16, 2004 at 06:49

Hi,

We are using in our project the STR710FZ2T6-Processor and have the following big Problem:

We need to program the PRCCU-block to obtain the outputfrequency RCLK of 28MHz (with a input at CK of 4MHz)

therefore we program the PLL1-Registers with the following Data:

PRCCU_PLL1CR=0x00000063 -> MX0=0/MX1=1(PLL mult. x 28), FREF_RANGE=1,DX2..0=011

PRCCU_CFR=0x00000009 -> DIV2=0, CK2_16=1, CSU_CKSEL=1;

With these port settings we expect a outputfrequency of 28MHz but obtain only 24MHz via the CKOUT-Pin of the CPU!

We checked out all ohter configurations of the MX-Bits. The outputfrequencies of the other MX-combinations are connect

(12/16/20Mhz).

What's going wrong? Is it not possible to get the right Frequency on a multiple factor of 28 (MX1=1, MX0=0) ? Are there any

workarounds or is the Chip not able to generate a Frequency with a multiple factor of 28 for the PLL1 ?

regards,

CEL-Team