2007-06-18 12:10 AM
2007-06-17 07:22 PM
Hi Bitter,
If you can attached your uCOS code project here. I can help you to take a look at what's the problem.2007-06-17 08:17 PM
ok.pls see attachment.
you can open UCOS_STR712_TCP.eww in IAR. ________________ Attachments : UCOS_STR712.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtJj&d=%2Fa%2F0X0000000aLX%2FOgiETC4XX6NI0XauBjhGXES.1T0Ql8VJcRwk_MzBIio&asPdf=false2007-06-17 09:20 PM
Hi bitter,
I did notice any problems with your uCOS code. Try testing your IAP or bootloader with the original uCOS example with only the changes for the software remap.2007-06-17 09:30 PM
ok.
I'll check the original IAP&Application Code2007-06-17 10:46 PM
hi tiger4
why you use -Z(CODE)INTVEC=VECSTART:+0xB8C in your test project need 0xbc byte?[ This message was edited by: bitter on 18-06-2007 11:28 ]2007-06-17 11:27 PM
-Z(CODE)INTVEC=VECSTART:+0xB8C is not set by me, it is part of the original code.
2007-06-18 12:01 AM
yahoooooo
I have sloved it。 because my IAP not use sys mode only usr mode thank u tiger.2007-06-18 12:10 AM
Haha...
you are welcome... 🙂