cancel
Showing results for 
Search instead for 
Did you mean: 

STHS34PF80 Sensor's Power Consumption is very high.

Sandesh42
Associate

Hello there,

I am currently working on a project where I am prototyping STM32WL55 with an STHS34PF80 sensor to detect the presence. The presence detection is excellent and robust so far. However, the power consumption seems to be very high at the moment. I am using Nordic Power Profiler Kit II to measure the power consumption of the STHS34PF80 sensor and it's around 350 microAmps. I am using Power Profiler as source mode sending 3.3v and measuring current consumption on the sensor. The TMOS Sensitivity is set at 2, AverageTAmbientNumber is at T_1, Block update is false, and TmosODR is running at 4Hz. I am using the Arduino framework to run the overall system and the sensor is purchased from Sparkfun (https://www.sparkfun.com/products/22494).

 

The power consumption is very high considering the sensor runs 24/7 and interrupts STM32WL55. I am using the library from SparkFun (https://github.com/sparkfun/SparkFun_STHS34PF80_Arduino_Library).

Any help would be highly appreciated. Thank you so much.

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Sandesh42 ,

Is this consumption measured by detaching the LED? Also, are you sure that the measurement is only on the sensor and nothing else is connected?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Federica Bossi 

Thankyou for your response.


This consumption measured is true without the LED. I removed the LED from the board and measured the current only on the sensor and nothing else is connected.