2004-06-28 03:17 AM
2004-06-27 11:37 PM
Hello
Can i use the Softec Indart for this device as ICP ? Thanks Latino2004-06-28 03:17 AM
For an external controller to be able to put the ST7SCR into ICC mode, the procedure has to be slightly modified because the ST7SCR has no external RESET pin to synchronize the start of the pulse train that defines ICC mode entry. For this reason inDART cannot handle the target's power supply in fact it is not able to reset the MCU in order to work in ''entry mode''.