2003-12-03 03:51 AM
2003-12-02 10:08 PM
Is the PWM output (OCMP1A) on Port F bit 4 effected by the DDR & the OR or does the the PWM write to the Pin/Pad directly.
I want an open drain output from the PWM. Is this achievable?[ This message was edited by: BrianM on 03-12-2003 11:39 ]2003-12-03 03:26 AM
When an alternate function is used , alternate function takes priority our standard I/O programming. When signal is coming from on-chip peripheral, that pin is automatically configured in O/P mode(push-pull or open-drain) depending up on the peripheral used. So, it is not possible to change this configuration.
2003-12-03 03:51 AM
Many thanks