Posted on June 19, 2009 at 05:25Hi I am using the ST Visual Programmer V3.1.1 along with the Raisonance device, I am currently working with ST7Flite29, the erase function is ''Greyed Out'' why is this, cannot seem to erase a device using this softwa...
Posted on February 17, 2009 at 06:26Are there any other forums around that are dedicated to st7 software, whilst this forum is ok, its not over active and can take a long time time to get a reply. :-[
Posted on February 10, 2009 at 13:27Thanks So as I have found as soon as you set the TIE flag it jumps to the interrupt You then load you data into SCIDR and Reset Int RIM keep doing this untill yoyr TX buffer is empty? Does this sound correct Re Br...
Posted on February 09, 2009 at 10:32Hi all I am writing a serial routine in assembler to TX some data using SCI. if I use the code in AN969 which is just a loop it works ok. But I want this to work with interrupts i.e. Send byte Do something When by...