2008-09-23 05:24 AM
2011-05-17 12:55 AM
Hi
I have problem with the new version of SSP example; If I use the SSP example n°2 from the new firmware library (12/07/2007), the master SSP0 sends data’s but the slave SSP1 doesn't receive data’s. The CPU stays in loop: while(SSP_GetFlagStatus(SSP1, SSP_FLAG_RxFifoNotEmpty)==RESET); But,when I used SSP example (05/18/2006 version), The master SSP0 transmits the buffer to the slave SSP1 Without errors. There are 32 errors when the slave SSP1 sends data to the master. The data’s received are the data sent to generate the clock. Thankx Yves from Brittany :-?2011-05-17 12:55 AM
Hi Yves,
Could you send more information (source code), At this moment, We (at least I) have a lack of details. Be careful, sometime, they are some error in ST example, resulting of a too fast copy past (a SSP0 where should be SSP1, for example) (i have a doubt about each example has been tested before releasing) Thanks in advance. Damien A french guy lost in the middle of the English Yorkshire 😉