cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP Parameters configuration

LPrat.3
Associate II

Could someone help to understand the better value to use at frequency deviation, considering at bellow specs:

 

#define BASE_FREQUENCY              916000000 //Hz
#define MODULATION_SELECT           MOD_2GFSK_BT05
#define DATARATE                    38400   //bps
#define FREQ_DEVIATION              ?????
#define BANDWIDTH                   100000  //Hz
#define CHANNEL_SPACE 180000  //Hz

 

A higher frequency deviation means that easier to read data from another devices (if frequency of devices drift)?

 

Best regards

Leonardo

0 REPLIES 0