2004-12-06 02:03 AM
RTC BIG PROBLEMS WITH INTERRUPTS
2004-12-05 11:30 PM
Hi guys !.
I'm starting to work with RTC of ST10 (F269), but I have some problems when I use both interrupts (AI and SI), in fact when boths are enabled only the SI works corretcly instead the AI doesn't arise !. I'm trying a simple program to obtain a led blinking of 1 sec (with SI) and a 15 sec blinking of another led (with AI). NB) I'm using Keil uVision 3 and in Debug mode (emulation) all seems to work correctly There is someone that can help me ??? I've attached the code. :-o :-o :-o :-o ________________ Attachments : RTC_CODE.TXT : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0NC&d=%2Fa%2F0X0000000bYA%2FP4WiiUETKPO4Wy.1MJJz5wdmP8xUR1xpIKv3W8V_IDY&asPdf=false2004-12-06 02:03 AM
Thanks Neila !
Now all Works and it's great !!!!!! :-D :-D :-D :-D :-D :-D