cancel
Showing results for 
Search instead for 
Did you mean: 

RTC BIG PROBLEMS WITH INTERRUPTS

yuri
Associate II
Posted on December 06, 2004 at 11:03

RTC BIG PROBLEMS WITH INTERRUPTS

2 REPLIES 2
yuri
Associate II
Posted on December 06, 2004 at 08:30

Hi guys !.

I'm starting to work with RTC of ST10 (F269), but I have some problems when I use both interrupts (AI and SI), in fact when boths are enabled only the SI works corretcly instead the AI doesn't arise !.

I'm trying a simple program to obtain a led blinking of 1 sec (with SI) and a 15 sec blinking of another led (with AI).

NB)

I'm using Keil uVision 3 and in Debug mode (emulation) all seems to work correctly

There is someone that can help me ???

I've attached the code.

:-o :-o :-o :-o

________________

Attachments :

RTC_CODE.TXT : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0NC&d=%2Fa%2F0X0000000bYA%2FP4WiiUETKPO4Wy.1MJJz5wdmP8xUR1xpIKv3W8V_IDY&asPdf=false
yuri
Associate II
Posted on December 06, 2004 at 11:03

Thanks Neila !

Now all Works and it's great !!!!!!

:-D :-D :-D :-D :-D :-D