cancel
Showing results for 
Search instead for 
Did you mean: 

Registers definition files for ST7FOX

radek
Associate II
Posted on February 01, 2008 at 06:04

Registers definition files for ST7FOX

2 REPLIES 2
radek
Associate II
Posted on January 31, 2008 at 19:29

Hello,

I have ST7VD 3.5.0 and I try to program an ST7FOX device, but I can't find registers definition files for FOX devices. Project wizzard supports FOX devices, programmer also, but 3.5.0 release of ST7VD doesn't have *.inc and *.asm files (in asm/include folder) for FOX devices. Where can I find this files? Do I have to write this files by myself?

Best regards,

Radosław Kwiecień

cheng
Associate
Posted on February 01, 2008 at 06:04

Hello Radzio,

I think these files are not yet available. Anyway, you can use some LITE products .h and .inc files for the moment as describe below:

FOXU0 -> ST7LITEU05

KOXK1/F1 -> ST7LITE49M

For the FOXK2 you can use the ST7LITE49M file but you have to add by yourself the register descritpion for the 16bits timer and for the SPI.

I hope it will help you.

Best Regards,

Cheng