cancel
Showing results for 
Search instead for 
Did you mean: 

RAM again

denis_sandrine
Associate II
Posted on July 03, 2004 at 08:48

RAM again

3 REPLIES 3
denis_sandrine
Associate II
Posted on July 08, 2003 at 05:06

Hi!

I have some questions!!!!!!!!!!!!!!!!!

Can you give some references of RAM compatible with the ST10F168?(16 bit demultiplexed)

Can you tell me more about the BHE signal?

I know that it is slower using external RAM than internal memory : do you know how much?

Thank you

guenther
Associate
Posted on August 07, 2003 at 15:11

Quote:

On 2003-07-08 08:36, sandrine82 wrote:

Hi!

I have some questions!!!!!!!!!!!!!!!!!

Can you give some references of RAM compatible with the ST10F168?(16 bit demultiplexed)

Can you tell me more about the BHE signal?

I know that it is slower using external RAM than internal memory : do you know how much?

Thank you

Take a look at the SAMSUNG K6R4016C1D-TI10 256kx16SRAM.

I use it with an ST10F269 @40MHz 16 bit demux Bus without any waitstates.

Works great up to now. Should work with your F168 too.
wjohnson
Associate II
Posted on July 02, 2004 at 13:21

How did you connect this RAM to the micro? We're hoping to connect like this (using an ST10F276 micro, basically the same as the 269)...

/WR -> /WE

/RD -> /OE

/BHE -> /UB

A0 -> /LB

We'd use a 16 bit demultiplexed bus. Would this allow us to write and read bytes and 16 bit words??