2007-03-23 12:07 AM
Problems with C Code Generation in PSDsoft Express
2011-05-17 02:51 AM
I have started to work with PSDsoft Express, and i 'm doing the example in the AN 1560. All is right, but in the moment when i must do the C Code, i have problems, when I push the bottom ''Generate C code, Specific to PSD''. It appears to me a pop up with this message ''Please check the website listed below for the latest firmware updates:'' and two links. These links are:
http://mcu.st.com/mcu/modules.php?name=Content&pa=showpage&pid=55 http://mcu.st.com/mcu/modules.php?name=Content&pa=showpage&pid=56 What is the problem, and what is the solution? I wish create a C code, but i don't understand if I must make the code with this option, or with Keil. Thanks very much.