Skip to main content
Associate III
August 27, 2024
Solved

Problem with generation PWM in Timer for STM32H750 (don't reach necessary frequency - 100 Mhz)

STM32H750 Discovery Kit board, Timer 1, Ch1 (PA8 output)

I used direct access to timer registers as a HAL library and the result was similar.

I can receive 10 MHz with direct access to register and   TIM1->PSC = 10;

But when  I set TIM1->PSC = 1 I don’t receive any signal from Timer1 with the next script 

 

"HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);

  RCC->APB2ENR |= RCC_APB2ENR_TIM1EN;

  TIM1->CR1 &= ~TIM_CR1_CEN;

  TIM1->PSC = 10;

  TIM1->ARR = 1;

  TIM1->CCMR1 &= ~TIM_CCMR1_OC1M;

  TIM1->CCMR1 |= TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2;

  TIM1->CCMR1 |= TIM_CCMR1_OC1PE;

  TIM1->CCR1 = 1;

  TIM1->CCER |= TIM_CCER_CC1E;

  TIM1->CR1 |= TIM_CR1_ARPE;

  TIM1->BDTR |= TIM_BDTR_MOE;

  TIM1->CR1 |= TIM_CR1_CEN;

  RCC->AHB4ENR |= RCC_AHB4ENR_GPIOAEN;

  GPIOA->MODER &= ~GPIO_MODER_MODE8_Msk;  // Clear bits

  GPIOA->MODER |= GPIO_MODER_MODE8_1;     // Set to alternate function mode

  GPIOA->AFR[1] &= ~GPIO_AFRH_AFSEL8_Msk;  // Clear AF selection for PA8

  GPIOA->AFR[1] |= 1 << GPIO_AFRH_AFSEL8_Pos;  // Set AF1 for PA8

 

 

I also adjusted A8 for  RCC_MCO_1 and received finally 100 MHz, so I can confirm that my oscilloscope works properly. 

And I found here that is possible to make 100 MHz for the timer for STM32H7 via timer and PWM

my settings are here 

and the same problem for other Timers 

as example 

HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_2)

static void MX_TIM15_Init(void)

{

 

/* USER CODE BEGIN TIM15_Init 0 */

 

/* USER CODE END TIM15_Init 0 */

 

TIM_ClockConfigTypeDef sClockSourceConfig = {0};

TIM_MasterConfigTypeDef sMasterConfig = {0};

TIM_OC_InitTypeDef sConfigOC = {0};

TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 

/* USER CODE BEGIN TIM15_Init 1 */

 

/* USER CODE END TIM15_Init 1 */

htim15.Instance = TIM15;

htim15.Init.Prescaler = 0;

htim15.Init.CounterMode = TIM_COUNTERMODE_UP;

htim15.Init.Period = 2;

htim15.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim15.Init.RepetitionCounter = 0;

htim15.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

if (HAL_TIM_Base_Init(&htim15) != HAL_OK)

{

Error_Handler();

}

sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

if (HAL_TIM_ConfigClockSource(&htim15, &sClockSourceConfig) != HAL_OK)

{

Error_Handler();

}

if (HAL_TIM_PWM_Init(&htim15) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim15, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

sConfigOC.OCMode = TIM_OCMODE_PWM1;

sConfigOC.Pulse = 1;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;

sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;

if (HAL_TIM_PWM_ConfigChannel(&htim15, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)

{

Error_Handler();

}

sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;

sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;

sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;

sBreakDeadTimeConfig.DeadTime = 0;

sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;

sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;

sBreakDeadTimeConfig.BreakFilter = 0;

sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;

if (HAL_TIMEx_ConfigBreakDeadTime(&htim15, &sBreakDeadTimeConfig) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN TIM15_Init 2 */

 

/* USER CODE END TIM15_Init 2 */

HAL_TIM_MspPostInit(&htim15);

 

}

 

This topic has been closed for replies.
TDK
TDKBest answer
August 27, 2024

You can change it in the GPIO tab on the left.

TDK_0-1724764260830.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

5 replies

TDK
August 27, 2024

Make sure pins are set to very high frequency. I bet the signal is there but with slow edges. What oscilloscope are you using?

"If you feel a post has answered your question, please click ""Accept as Solution""."
RonilAuthor
Associate III
August 27, 2024

Hello, thank you, I use PicoScope6404D (500 Mhz)

what do you mean about - "Make sure pins are set to very high frequency. " I use a timer and PWM and made only "Fast Mode" - Enable

TDK
TDKBest answer
August 27, 2024

You can change it in the GPIO tab on the left.

TDK_0-1724764260830.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
RonilAuthor
Associate III
August 27, 2024

ohhhh, it is works now, thank you so much, my god how did I miss this!!