cancel
Showing results for 
Search instead for 
Did you mean: 

Pocket Flash Device

mailtoarup
Associate II
Posted on December 11, 2003 at 02:49

Pocket Flash Device

5 REPLIES 5
mailtoarup
Associate II
Posted on December 10, 2003 at 04:09

hello,

i got a pocket flash device from ST MicroElectronics from seminar which was attended by one of my friend,which contains seminar material.Now to see the contents i have to connect it to USB port and for running it i have to download some sriver software for this.Pls tell me exactly where can i find the driver and how to down load it .and how to see the content..as i have never use such device...

pls tell me in detail...all the file needed to opening up the content...

thanks,

arup

alain2399
Associate II
Posted on December 10, 2003 at 05:41

You need a driver only under Windows 98. Under Win 2000 and XP they are provided by Windows and it works automatically, i.e Windows explorer detects and mount the PFD and a remmovable drive.

jatin
Associate II
Posted on December 10, 2003 at 07:22

Just connect it to the USB port and use it.

mailtoarup
Associate II
Posted on December 11, 2003 at 01:24

hai,

i m using windows 98.Now tell me if i connect that memory device to

USB port then without loading any driver will this work.

i just want to be sure for safety purpose as i have no idea of using such type of device.

thanks,

arup

jatin
Associate II
Posted on December 11, 2003 at 02:49

Yes, if you are using Windows98 then you will have to install the driver. Download ''Windows 98/ME driver Installer package'' available on the same site.