2007-05-30 04:28 AM
Original Short Range RFID DemoKit firmware on upsd3422ev does not compile
2011-05-17 02:51 AM
Hello, I got the demokit with upsd3422ev, and the code (firmware) supposed to be working on the processor.
Teh 1st thing I did was to launch the Build of the code and the problem is that the code (without updating anything) is failling under Keil Build process. I got this error message: <assembling STARTUP34.A51... compiling appli.c... compiling autonomous.c... AUTONOMOUS.C (934): error C249: 'DATA' : SEGMENT TOO LARGE compiler Encoder.c... ... >> Does someone has any idea about what is failling? Is there any update of this code somewhere? I attached the screenshot of this error Thank you in advance! :) fabrice :p [ This message was edited by: tiofabby on 30-05-2007 17:14 ]