2005-03-07 07:23 PM
My STPC SBC won't boot to CE desktop with Ethernet cable connected
2005-01-19 07:59 AM
My STPC Consumer-II SBC won't boot all the way into the CE desktop if I first power up board with Ethernet cable connected. If I wait until the SBC boots into CE desktop and then connect an Ethernet cable, everything works fine. I get an IP address, and I can browse the Internet fine. I know the Ethernet cable is okay because I tested it on a nearby PC. Also, I do not have ''Boot from LAN'' enabled in the BIOS only boot from hard disk. I think that CE is trying to do something on the network before everthing related to the ethernet is loaded and configured. Therefore, it must be hanging because of this.
Thanks for any help, Joel2005-03-07 07:23 PM
Hi,
Which network adapter are you using ? Which network configuration are you using? Which is the version of CE that you use ? Tanks.