Posted on January 19, 2005 at 16:59My STPC Consumer-II SBC won't boot all the way into the CE desktop if I first power up board with Ethernet cable connected. If I wait until the SBC boots into CE desktop and then connect an Ethernet cable, everythi...
Posted on January 19, 2005 at 16:47Thanks for the suggestion, and you're right. it was a PC104 board configuration problem. The Default Video Memory Size was set too low (1.0M). I set it to 4.0M, and the video works fine now. Joel
Posted on January 14, 2005 at 17:40I have been trying to get the video working on an Advantech PCM-3348F PC104 SBC under Windows CE 5.0 but to no avail. This SBC utilizes an STPC Consumer-II Processor. I've installed ST's Win CE 5.0 Consumer-II BSP ...