cancel
Showing results for 
Search instead for 
Did you mean: 

memory model and link command file settings of ST72F521

csameling
Associate II
Posted on May 12, 2004 at 05:56

memory model and link command file settings of ST72F521

10 REPLIES 10
csameling
Associate II
Posted on May 12, 2004 at 05:56

hi sjo,

it is a mistake of me: I do not use IAP but ICP (In Circuit Programming)!!!!!

There is no need to keep my application running during programming.

But there is one error if I use it with the datablaze. If the software is downloaded on microcontroller and I take off the connector of the programming tool (inDart-ST7F) my application do not run.

Is there any settings which I can change that the application is running (also after voltage breakdown)?

chris