2007-05-06 10:03 PM
2011-05-17 12:42 AM
Hello ST
I have tested the STR912FA with respect to power consumption and I have seen some improvement since STR912F. On the FA version I have measured 0.067mW on the core(1.8V), and 2.3mW on I/O(3.3V), but in the datasheet it specifies: ''Sleep Mode as low as 50 uA''. What does i mean in mW? Is it only the core? What can I do to lower the power consumption on the 3.3V? (I have currently disablet every pheriferal except SCU and RTC) Thanks /jl