cancel
Showing results for 
Search instead for 
Did you mean: 

Lite02, LiteS2 RCCR recovery in the event of removal of readout protection

rk-system
Associate II
Posted on February 19, 2007 at 06:22

Lite02, LiteS2 RCCR recovery in the event of removal of readout protection

2 REPLIES 2
rk-system
Associate II
Posted on February 07, 2007 at 11:32

Hi! In my own programmer I'm trying to recover RCCR calibration bytes after removing of readout protection in ST7Lite02 and ST7LiteS2. I'm relying on following documents: ''Quick Reference Manual'' (chapter 1.2, page 3/9) and ''ST7 Family Flash Programming Reference Manual'' (chapter 2.2.1.3, page 16/68). Described procedure of RCCR[0,1] restoring bases on reserved memory locations F960h/F961h (or DEE0h/DEE1h in Lite1x, Lite2x).

Reads from these cells always return values 00h. Is there any special procedure to read calibration bytes from mentioned locations?

Thanks for help!

I'm attaching source of driver used to reading bytes via ICC

[ This message was edited by: Michal on 07-02-2007 16:12 ]

________________

Attachments :

code.asm : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Bl&d=%2Fa%2F0X0000000bVd%2F8Wlqs1gPIvh6S1HXB2cONJXrgASma5z.4RJU07ZLiHQ&asPdf=false
rk-system
Associate II
Posted on February 19, 2007 at 06:22

Problem solved, thanks anyway.