2023-05-22 06:05 AM
2023-05-22 06:19 AM
Welcome, @Subhash, to the community!
even if this were possible, why would you want to change a SPICE model?
It is originally designed to represent the real data of the MOSFET in a simulatable form. If you change this data, the model no longer corresponds to the physical device and can only be investigated theoretically and the result is no longer practically relevant?
Regards
/Peter
2023-05-22 06:52 AM - edited 2023-11-20 04:54 AM
Hello @peter BENSCH
I want to check switching behavior of MOSFET with various Vth voltage (as mentioned Vth range in datasheet). I am doing simulation on this part number: SCT012W90G3AG_V3 in LTspice. Datasheet shows range of VGS(th): 1.8 V(min), 3.1V (typ.) and 4.2V (max) as per following snapshot.
And I also observed one specific note on spice model like dR=0 dVth=0 dVsd=0 dCi=0 dCr=0 dCo=0.
Could you tell me, why this one is given with spice model?
Regards,
Subhash