2006-03-16 03:23 AM
2006-03-15 04:56 AM
Hi
I try to use the sample code in VB6 delivered with this library (downloaded from softec.com). My application is based on ST7Lite When I try to connect my ST7 and the indart-STX card (USB), I have the message ''Hardware protection key not found'' ??? what does it meens ? If I use my favorite indart STVD7 and try to connect my ST7 card using the indart-STX it work !!! So, in my mind it is not a configuration problem... USB drivers for indart-STX are properly installed as with indart delivered application's all is fine ;-) ! But I need to use the ipl_st7 library to develop my own programmation module. Help me please Jean-Marc :-) ________________ Attachments : ipl_sample.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzOz&d=%2Fa%2F0X0000000bVk%2FhluugDRR8KxRJG.Dm38lPeF0cNPCMxTljxeYWDzvb90&asPdf=false2006-03-15 09:43 AM
It means you have to pay to use the library, or try and get a demo licence.
Regards sjo2006-03-16 01:02 AM
I don't think so... this library is free, u can download it direcly from softec home page.
2006-03-16 01:34 AM
Free to download but not use.
This is mentioned in the user manal, it uses a usb dongle Regards sjo [ This message was edited by: sjo on 16-03-2006 15:06 ]2006-03-16 02:59 AM
ur rigth :-W I haven't read this part....
Where I can buy this dongle ??? thanks !!!2006-03-16 03:23 AM
You could always try the same place you downloaded the software from - www.softecmicro.com
Last time i enquired it is expensive. Have you thought of a lower cose solution, ST programming API (free) and a RLINK programming tool, instead of the indart. Regards sjo