Posted on September 15, 2006 at 11:51Ok !! it works! The problem come from the DEVIDE name you must pass to the IPL_OpenCommunication function! Function comming from the IPL library! I was programming the ST7lite39 as a ST7lite29! Setting the device...
Posted on September 14, 2006 at 06:49Hi, I'am developing my own application based on ST7LITE39. I use the inDART-STX for ST7 with Softec STVD7 debugger 3.11 to program my target. And as described in the softec FAQ (14) see below, I can use RC oscill...
Posted on March 15, 2006 at 13:56 Hi I try to use the sample code in VB6 delivered with this library (downloaded from softec.com). My application is based on ST7Lite When I try to connect my ST7 and the indart-STX card (USB), I have the mess...