2005-02-06 06:31 PM
interfacing st72f264 & 93C46 spi eeprom -problem
2005-02-06 06:31 PM
Dear sir,
I am facing a problem with SPI.I am trying to interface ST72F264 mcu with 93c46 spi eeprom.I am using SPI port of the mcu.My con. in my application board is like this. /ss pin is software configured as master(SSM=1;SSI=1) MISO & MOSI tied together and connected to DI & DO(which are connected together) pins of the eeprom(as i will either transmit or receive data). SCK-PB6 is connected to pin2(SK) of 93C PB3 is connected to CS of eeprom(for slave selection) Now just for testing i m sending a byte.I have selected x16 organization of eeprom.First I have send writeenable command,then write 2byte of data(d15-d0) at memory location 00 and read the same (as per datasheet).As i m not able to get what i have written thro READ com command,so i am doubtful about my communication with the eeprom?? Any suggestion on my circuit arrangement & procedure for communicating will be highly appreciated.I have gone thro AN9 Pls if possible i need some code to communicate with 93C making PB3 at high state. EWEN 1stbyte:00000100 2ndbyte: 00110000 (as per datasheet) WRITE 1stbyte:00000101 2ndbyte: 00000000(address a5-a0) 3rdbyte:00000000 & 4thbyte:00000000(data d15-d0) READ 1stbyte:00000110 2ndbyte: 00000000(address a5-a0) then i read 3rdbyte & 4thbyte(data d15-d0)..not getting anything I have attached the code file ''spi_code.txt''. Thanks & Rrgards, Arup null I have attached the code file ''spi_code.txt''. ________________ Attachments : spi_code.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0EA&d=%2Fa%2F0X0000000bVl%2Fi7R2XDtKTfCn8uNDNfSan3yzd2QhjCUg9NJPurNOISE&asPdf=false