2003-03-02 09:43 PM
inDART-ST7/521 kit : can not get out from the Cosmic startup file, crtsx.s
2003-02-12 09:26 AM
I have an inDART-ST7/521 kit configured to target a ST72521R9T. At first, I used V1.05 then I recently switched to V1.0.9.
For both versions, I noticed that my ST72521 program was sometime stuck in the crtsx.s startup file (I use Cosmic). Other times, I have some communication errors using STVD and Data Blaze. I am sure of my Cosmic code because I have tested it on a ST7 EMU3 emulator. My Indart kit is also brand new. Any idea to explain these 2 issues ? Jojo2003-03-02 09:43 PM
When you say you're stucked in the startup file, does that mean stuck on a particular source code line or stucked because of a reset for instance? Check if you're configured in H/W WDG for instance (or place a breakpoint on the first line of the startup to see if the program performs reset).
Do not hesitate also to ask support from Cosmic or Softec!