2012-01-04 01:12 AM
I use ST7MC1K2B6 to control a BLDC motor with sensorless .
when I boost voltage to 200V, MCU is reset. I don't use LVD and WDG, I just use a POR(Power On Reset,20k/10uF). I change the RC parameter, but improvement is not obvious. How to identify the reset source? Is it beacause of EMC? If it is because of EMC, how can I solve this problem? #identify-the-reset-source-2012-01-11 05:21 PM
disappointing, no one answer me!