cancel
Showing results for 
Search instead for 
Did you mean: 

How to force D event to open Z window

kbandudej
Associate
Posted on July 19, 2012 at 05:39

Refer to AN1130 on page 15, 

''If the motor speed is suddenly increased by the user so the Z event will happen earlier. If BEMF signal is already be positive when the phase extremity becomes a floating point thus the signal will not cross the threshold voltage and the ST72141 will not detect the End of demagnetisation event. As a consequence, the ST72141

won’t open the Z event detection window.

We force an End of demagnetisation event and so the Z window detection is opened in all cases.''

Can someone please explain how to detect Z event before End of D is not finish yet? and how/when we can force D event in this case?

Do you have timing diagram of phase current and phase voltage similarly to figure 9. in case of Z event is happen early.

Thanks.
0 REPLIES 0