2008-06-13 05:28 AM
2011-05-17 12:42 AM
Professionals where are you ?
Gurus of STR9xx where are you ? If you have flash programming example please send it. But not the example from library (thats runs from ram). Need example that runs from flash.Please...2011-05-17 12:42 AM
Hi,
I do not know if this is your problem (I am not a Guru..), but you must keep in mind that writing to flash with a FMI_clock > 25MHz will give you unexpected results. So before writing to flash, yoy have to reduce the CPU clock-frequency. See datasheet errata 1.21 at page 11! Regards Luc Vercruysse2011-05-17 12:42 AM
In Keil STR91x.s file i set MCLKSEL = fOSC (8 Mhz) it must be sufficient.
Also i tried to set MCLKSEL = fPLL (PLL =24 Mhz), PLL ENABLE, FMI clk = Rclk/2 (project work from ram but from flash it not work yet). I do some mistake but can not find it ?2011-05-17 12:42 AM
Is the code you are talking about ''example1'' from previous post ?
If not, post it here please, i will have a look. Luc2011-05-17 12:42 AM
Yes Example1 is the needed project. On my hardware when i compile it
to Flash area (to run from 0x0) it not work but when it run from RAM it work as expected. Thank you for help. Please answer me and explane me what is my mistake.2011-05-17 12:42 AM
There is nothing wrong with this code. But check your memory assignments.
This should be the same as the attched file. Regards Luc.2011-05-17 12:42 AM
As i understand you changed the parameters (untitled.bmp) and this project(EXAMPLE1) work from flash on your hardware.
2011-05-17 12:42 AM
Thank you it work the problem was(Thumb mode).In my project i choosed ARM mode. Yet i do not know why it affect to flash writing but it work and it's
super. Thank you. Good luck in your development board creation.2011-05-17 12:42 AM
Thank you Zouh yet i do not know the difference . In thumb mode it work
and it's OK. If you can explane the difference i will be thankful.