cancel
Showing results for 
Search instead for 
Did you mean: 

FIT rate of M93C66-A125

cchoi.1
Associate II

Hi, Please check FIT rate of M93C66-A125 component!!!

Thank you!!

5 REPLIES 5
Pierre P.
Senior III

Hi,

At 55°C:

1.2 - 60% confidence level

2.9 - 90% confidence level

BR

Pierre

Thank you for your quick reply.

Additionally, I would like to know the description of the failure mode.

For example, open mode : ??% / close mode : ??%..

Thank you!​

Pierre P.
Senior III

Hi,

I've no data on that.

BR

Hello.

I want to know FIT rate, Failure Mode and Failure Mode Distribution Rate​.

Thank you!

What is the failure rate from the users​ inability to use the part, due to lack of integrity checking, redundancy and recovery methods?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..