2005-06-06 12:41 AM
facing problem in programming external flash in str710 evaluation board
2005-06-03 08:51 PM
Hi every one
i am trying to program a bin file in the external flash in str710 evalution board using realview ice-ME via jtag but not succeding sequence followed: 1.ttings did on board: Ram boot mode (sw14 at 1-2,sw15 & sw13 at 2-3). 2.Powered on board. 3.Run RVDEBUG software on pc. 4.Clicked ''Connect Target'' and it connected 5.Clicked Debug>memory rigister>upload/download memory 6. filled x.bin file name and memory address (0x60000000)in the dialog appeared. 7.Selected ''load memory from file'' option. in same dilog 8.selected type as ''Raw'' 9.Clicked Apply. 10. command appeared at output window but no confirmation or error massage got . 11. then selected option ''varify file'' in same dilog with all settings same. 12. Got error response'' memory missmatch at 0x60000000'' So any help in this regard will be appreciated. jeetendra2005-06-05 08:36 PM
Hi jeetendra,
Please can you tell me if you use the last version of the FME files, if yes be sure that you are connected under ST-STR710-EVAL. Cheers, Hich :p2005-06-05 08:40 PM
i got the problem actually there is no fme file for evaluation board external flash and even there is no entry for the external flash in the bcd file .
so i did the entry in bcd file but i still required fme file for the extarnal flash.2005-06-05 09:53 PM
Dear ibtiss
thanks for your response i already used st710-eval for connection and failed to program external flash. after that i checked bcd file for st710-eval , in that file there is no entry for the external flash. i studied an110 of arm and inserted an entry into the bcd file for external flash. but i need fme file for the external flash used in the board. best regards jeetendra2005-06-05 10:45 PM
Dear Ibtiss
the RVDK version is 1.6.1 Regards Jeetendra2005-06-06 12:41 AM
Thanks ibtiss
loaded successfully best regards jeetendra