2010-01-12 03:06 AM
2011-05-17 12:45 AM
I have a 512k by 8 bit SRAM interfaced to an STR912FW44 via 8-bit multiplexed mode using CS0. Whenever I write a byte to it, it writes the same byte into 4 locations in the SRAM two bytes 10 hex apart in two places 100 hex apart. What am I doing wrong? The compiler is keil C.
2011-05-17 12:45 AM
Hi All,
Does anyone found why CS0 is activated 4 times in 8bits (or even 16!!) mux mode when writing a single byte at a single location ??? I did not found any chronogram for this mode ?? With the same configuration on CS1, CS1 is activated correctly one single time ?!! regards,2011-05-17 12:45 AM