2007-01-19 12:07 PM
Early breakpoint dosen't prevent startup code from beeing executed
2007-01-07 10:39 PM
I have a STR7 dev. board with a JTAG debugger attached and are using Multi 2000 dev. environment. If I set a breakpoint early in the code, it dosen't prevent the startup code from being processed. It seems that the processor starts running after reset, and the debugger then creates a connection afterwards, this means that some hardware are initialized before I would want it to!
Is it the STR7, the debugger or the debugger software that has a problem? PS: It works fine on the Atmel AT91 we used before! [ This message was edited by: T-Bee on 22-01-2007 08:37 ]2007-01-19 12:07 PM
Dear T-Bee,
You have to check if you are booting from the right hardware boot mode Internal Flash, internal RAM or external Flash/RAM if you are using STR710 device and to ensure that your compiler / debugger is loading the firmware code accordinately. I think, it is a problem of the debugger / software debugger because each toolchain from a lot of vendors are not the same.So each one implements a different scheme of breakpoint handling mainly from the flash memory( like using SWI ) etc... Another Point also is that the debugger has to Reset the micro using a software JTAG reset before that the CPU has excecuted some startup code and most of debuggers introduces some delay in this start-up phase. I hope that this may help you :-) regards, Rave :-o [ This message was edited by: Rave on 21-01-2007 17:39 ]