2006-04-26 11:52 PM
2006-04-20 12:28 AM
Hi,
we expect to use a STR710F in a USB device. For this reason we should use a 16MHz external clock generator (multiplied by factor 3 to reach the 48MHz USB sampling clock). My question is: is possible to run the ARM core at higher speed than 48MHz e.g. 64MHz in a device having a singel 16MHz clock source? thanks2006-04-26 07:57 PM
Hi RISC,
thanks for your answer, but I am still little confused. The approach is to feed the same external clock source to both PLL1 and 2 inputs ?2006-04-26 11:52 PM
thanks.