Posted on July 14, 2006 at 10:13Hello all, I am confused, on Table 26 of the Reference Manual for the STR71x Controller Family there are 16 int sources. In the introduction doc on Table 3 there are two more interrupt pins P1.12 and P1.15. Which Tabl...
Posted on April 27, 2006 at 04:57Hi RISC, thanks for your answer, but I am still little confused. The approach is to feed the same external clock source to both PLL1 and 2 inputs ?
Posted on April 20, 2006 at 09:28Hi, we expect to use a STR710F in a USB device. For this reason we should use a 16MHz external clock generator (multiplied by factor 3 to reach the 48MHz USB sampling clock). My question is: is possible to run the AR...
Posted on March 30, 2006 at 11:45Hi everybody, i am wondering about the data in the specification of the ''STR71x MICROCONTROLLER FAMILY'' there is ISO 7816-3 asynchronous protocol specification that does not match to the Data in this spec. ETU Data...