cancel
Showing results for 
Search instead for 
Did you mean: 

Can STR911FAW47 used to replace STR911FAW44 without change in hardware & firmware?

fwu2
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Even if the thread is older, here is a short answer that may help others.

Yes, this should be possible, if the user program does not rely on the product id and/or rev level, because the replacement just provides more memory.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Even if the thread is older, here is a short answer that may help others.

Yes, this should be possible, if the user program does not rely on the product id and/or rev level, because the replacement just provides more memory.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.