2005-03-10 06:20 PM
2005-03-06 09:22 PM
Hello,
I have a pb with my adc conversion. Here is attached the schematic. When Vin is under 4V I have a good conversion. But when Vin is more than 4V, there is a saturation at 4.2V. Here are the measurements : Vin= 1V ADC measurement = 1V 3V 3V 4V 4V 4.3V 4.1V 4.5V 4.13V 5V 4.2V I checked Varef and I have 4.998V. I've also tried with minimum ADC frequency and maximum sample time so the condensator can charge itself during the maximum time possible. So I don't understand why I can't measure a voltage more than 4V :-W. I have the same pb with all my boards, so I don't think it's a component (ST10F168) failure. Does anyone has an idea?? Thanks, Steph ________________ Attachments : ADC_in.doc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Nc&d=%2Fa%2F0X0000000bYo%2FJfWet_rTbQDNp5ZIv2WndTFgPt3DB44mlK7mlJaTnws&asPdf=false2005-03-08 09:01 PM
Hello,
Try to remove the Zener diode and verify if the problem persists.2005-03-08 10:00 PM
thanks for your reply... but I tried without no Zener and no Capacitor, and I have the same problem.... The fact is, I measure 5V at the AN in!!!!!!! So I was thinking about a bit to change in a register..........
The pb still to be solved...... @++, Steph2005-03-10 06:20 PM
Hello,
I finally found where the pb came from : the op amp I was using to generate the signal to convert wasn't a rail to rail and had a 4.3V saturation. So, nothing to see with the ST10!!! Bye, Steph.