2003-07-09 06:37 AM
2011-05-17 02:54 AM
Hello,
ON the DSK3200 Kit, Which is the FREE addressable memory space on A/D bus? it's from 0x4000 to 0x7FFF or not ? How can I access into ? (xdata, xbyte ???) thanks2011-05-17 02:54 AM
The uPSD A/D bus can directly address up to 64K (0 - 0xffff) and the remaining memory can be addressed via memory paging, please see our application note, AN1560, from our website. Also you may want to take a look at our design examples on the same website, that uses the xdata memory access.